Technical Articles
Measuring the Efficiency of Diffraction Gratings
While simple in principle, measuring the efficiency of diffraction gratings is a complex process requiring precise methods to achieve acceptable results. Every optical, mechanical, and electronic component comprising an efficiency measuring system is a potential source of error. Environmental factors may also contribute to the overall measurement uncertainty.
Technical Articles
Diffraction Gratings - The Crucial Dispersive Component
A grating disperses light incident on it. Dispersion is the phenomenon by which a spectrum of light is separated in space by wavelength. Prisms also disperse light by wavelength and can be used in spectrometers, though grating-based dispersing instruments offer a number of advantages so few commercially available instruments use prisms.
Technical Articles
Meeting Measurement Challenges For Low-Power, Pulsed, or Modulated Light Sources - Photonics Online
It is particularly challenging to measure a low-average-power pulsed light source, such as an LED or a low-power laser diode, especially when the electrical designers do not know the detailed optical characteristics of the light source.
Technical Articles
Motion Control Systems Gain Flexibility - Laser Focus World
Complete motion-control systems are now available that are readily programmable for multiple applications of positioning equipment.
Technical Articles
Motion Specifications Don't Always Tell the Whole Story - Laser Focus World
Understanding what's behind a specification, the measurement and the analysis, is critical to obtaining consistent motion-control performance.
Technical Articles
Optical Mounts: Ignore Them at Your Peril - Photonics Spectra
Optomechanical mounts may seem like insignificant design elements, but they can make or break a photonic application.
Technical Articles
Optical Table Basics: From Breadboards to Active Vibration Control Systems - Laser Focus World
Setting up an optical laboratory begins with specifying the optical table, a task more complex than it sounds. Understand your requirements before you place an order.
Technical Articles
Photonic Crystal Fibers Have Many Uses - Optoelectronics World
Advances in photonic-crystal-fiber technology promise to yield not only better ways to guide light, but more efficient fiber lasers as well.
Technical Articles
Proper Load Distribution Ensures Stable Operation
With vibration-isolated platforms, questions of load distribution and static stability of pneumatic support systems are not always properly understood. This can create difficulties when setting up modern optoelectronic systems.
Technical Articles
Vibration Isolation in Optical Test Systems - Photonics Tech Briefs
A common source of instability within a light beam path is vibration. Vibration control systems that include, typically, vibration isolators and optical tables, are intended to minimize the impact of environmental vibration.
Technical Articles
How To Minimize Measurement Errors In Solar Cell Testing - Solar Industry
Research using properly measured solar reference cells can be transferred to new technologies for full-scale modules.
Technical Articles
Standards For Simulators Can Vary Widely - Solar Industry
The differences among the three standards used for evaluating solar cell performance might create confusion during testing.
Technical Articles
Specialized Systems Characterize Laser Diodes - Laser Focus World
Device sensitivity to temperature, current, and voltage must be accounted for when designing laser diode test systems.
Technical Articles
Specifying Fiber Alignment System Performance: Coupling Loss Offers An Alternative to Motion Capability - Motion Control Tech Briefs
One of the most difficult assembly tasks ever introduced into commercial manufacturing is the sub-micron alignment and attachment of a fiber-optic to a laser diode or other optical waveguide.
Technical Articles
Spectral Processor and ASE Source Aid Fiber Sensing - Laser Focus World
A broadband amplified-spontaneous-emission fiber source and programmable spectral processor combine to enable wavelength-multiplexed fiber sensing with great flexibility.
Technical Articles
Table Improves Optical Systems from Ground Up - Laser Focus World
Photolithography and the semiconductor industry are facing a critical juncture. The 32 nm node is only a few years away, and next-generation methods for patterning the even-smaller, sub-30-nanometer-scale dimensions on silicon wafers at the node beyond that are unproved.
Technical Articles
The Top Five Motion Application Mistakes and How to Avoid Them
Recognizing and avoiding common errors will better prepare users of precision motion control devices to make purchasing decisions and may substantially improve application results.
Technical Articles
Tunable Diode Lasers - Lasers & Optronics
Tunable diode lasers are increasing their market penetration via rapid evolution with a new generation of products every year or so.
Technical Articles
UHV Environments Require More From Motion Systems - Laser Focus World
As the number of applications for ultrahigh-vacuum (UHV) environments increases, motion systems must be modified to manipulate optics, particle beams, and measurement devices inside UHV chambers.
Technical Articles
Better Test Systems Boost Laser Diode Performance - Photonics Spectra
As laser diodes continue their drive to the head of the class, instrumentation that provides test and measurement support is not far behind.
Page 1 of 3