Manuals

Manual

ESP301 User Manual

This manual provides descriptions and operating procedures for the integrated 3 axis ESP301 Controller/Driver (ESP = Enhanced System Performance).

Manual

BG Goniometric Cradles User Manual

BG Series goniometric cradles rotate on a transverse axis above the platform. Compared to full 360° rotation stages, they offer maximum access to the rotating part and allow construction …

Manual

IMS Linear Stages User's Manual

The IMS Series linear stage complements the ILS Series by providing longer linear travel ranging from 300–600 mm.

Manual

MTN Linear Stages User's Manual

The MTN Series linear stages are durable, all-steel construction linear stages with excellent stiffness, load capacity and thermal stability.

Manual

Oriel Cornerstone 130B Monochromator User Manual

The Oriel CS130B 1/8m monochromator is a high performance, economical, and user-friendly instrument that is ideal for research and OEM applications.

Manual

BG Goniometric Cradles User Manual 2

BG Series goniometric cradles rotate on a transverse axis above the platform. Compared to full 360° rotation stages, they offer maximum access to the rotating part and allow construction …

Manual

XM-S Linear Motor Stages User's Manual

The XM Series of ultra-performance linear stages delivers dynamic performance capable of consistent, reliable motion to 1 nm. This positioning capability makes them ideal for various …

Manual

ILS-LM-S Motor Stages User's Manual

The ILS-LM-S Series linear stages are designed for self-supporting applications with travel ranges from 100 mm to 300 mm.

Manual

URS Rotation Stages User's Manual

The URS family of rotation stages is ideal in applications which require an all-around rotation stage in terms of positioning performance and cost.

Manual

Delay Line Stages User Manual

The DL linear stages Series is a high performance but very affordable, linear motor driven with an integrated motion controller. This manual provides operating instructions for the …

Manual

IDL280-Z20 Vertical Stage User's Manual

The IDL280-Z20 provides fine MIM, smooth motion for fine positioning and stiff construction for use with high dynamic performance XY systems and is the ideal stage for industrial applications …

Manual

MTN-BLHS Linear Stages User's Manual

MTN-BLHS are reliable all-steel construction stages with excellent stiffness, load capacity and thermal stability, ideal for applications that require moving heavy loads at high-speed …

Manual

FC Stages Controller GUI Manual

The purpose of this document is to provide instructions on how to use the FC Series Controller graphical user interface (GUI). The FC Series GUI is a graphical user interface, that …

Manual

FCR100 Rotation Stages User's Manual

This manual provides operating instructions for the FCR100 intelligent stepper motor rotation stage that you have purchased. The FCR100 is a precision rotation stage with an integrated …

Manual

FCL Stages User Manual

The FCL is a precision linear stage with an integrated stepper motor/controller. The stage can be easily controlled from a PC, using a downloadable graphical user interface (GUI).

Manual

URB100CC Rotation Stage User's Manual

The URB100CC rotation stage is based on our popular URS series, but features a belt drive instead of a worm gear.

Manual

Delay Line Stages Controller USB Driver Installation Manual

The DL controller uses the “Communications and CDC Control” USB-IF class. The driver for this USB class is included in windows but a custom file .inf is needed for windows 7 and 8.

Manual

Delay Line Stages Controller LabVIEW Drivers Manual

The purpose of this document is to provide instructions on how to use DLS LabVIEW library. The Windows PC computer requires having the .NET Framework installed.

Manual

Delay Line Stages Controller Command Interface User Manual

The Delay Line family of affordable linear motor driven stages is optimized for ultrafast spectroscopy applications that require repeatable and precise delays (0.5fs).

Manual

Delay Line Stages Controller GUI Manual

The DL Controller GUI is a graphical user interface (GUI) which allows the user to interact with the DL controller that is connected to stages. The user can initiate moves, change the …

Page 1 of 19